Setting a default Alarms view

The default Alarms view is the view that opens when you first open the Alarms application. You can set a default for your own workspace or the entire system.

NOTE: Access to this application or function is controlled by user privileges. See Managing user accounts, role names, and mapping for details.

To set a default Alarms view:

  1. In the alarm viewer, open the View Library and navigate to the view you want to set as default.
  2. Right-click the view name or click Options for this view, and select Set as default. This opens the Configure Default Item dialog.
  3. In Configure Default Item, enable Set as my default or Set as system default.
  4. Click OK to save the default settings.

For information on how to use Alarms, see Alarms.