Viewing alarms
View Alarm Status to assess the state of the monitored power system and to respond to important events and issues. View Alarm History for root cause analysis and to understand the sequence of events.
To view Alarm Status or Alarm History:
- In the alarm viewer, open an existing alarm status or alarm history view from the View Library, or add a new View.
- View the alarm information displayed in the alarms display pane.
(Optional) In the View Library, right-click the view name or click Options, and then select Edit to open the view settings. You can also open the view settings by double-clicking the view name. Adjust the settings for View Type, Priority, State, Sources, and Categories to customize the view if necessary. Save the modified view settings or click Cancel to discard the changes.
For information on how to configure Alarms , see Alarms configuration.