Settings and Diagnostics UI
Settings and Diagnostics consists of the Notifications Settings configuration, migration, diagnostics, and licensing features and information.
| 1 | Settings navigator pane. Click a setting category to work with that setting. For more information, see Configuring Notifications. |
| 2 | System diagnostics and settings. For more information, see Troubleshooting Notifications. |
| 3 |
The server's license status. |