Profile Editor main menu options
The main menu options (File and Settings) on each of the major tabs of the Profile Editor are described in the following table:
| 
                                                         Field Name/Valid Entries  | 
                                                    
                                                         Comments  | 
                                                
|---|---|
| 
                                                         File > Save  | 
                                                    
                                                         Saves any current changes.  | 
                                                
| 
                                                         File > Create CSV file  | 
                                                    
                                                         Creates a CSV file of basic tag data. Store the file in a folder you designate. The file can be viewed in Excel.  | 
                                                
| 
                                                         File > Print Tag Selections  | 
                                                    
                                                         Displays a print preview of all of the tags for this device type. You can then print the spreadsheet.  | 
                                                
| 
                                                         File > Import  | 
                                                    
                                                         Import projects from other instances of the Profile Editor. These must be PLS or ICD files. For more information, see Import and export project files.  | 
                                                
| 
                                                         File > Export  | 
                                                    
                                                         Export a PLS or ICD file to be used in another instance of the Profile Editor, or to be used as a backup. For more information, see Import and export project files  | 
                                                
| 
                                                         Settings > Display Advanced Properties  | 
                                                    
                                                         Causes additional “advanced information” columns to display.  | 
                                                
| 
                                                         Settings > Remove Import Templates  | 
                                                    
                                                         Delete any import template that has been added to the project. To add import templates, see Using import templates.  | 
                                                
| 
                                                         Settings > Set Up Custom Tags  | 
                                                    
                                                         Displays the Add/Edit Custom Tags screen. See for a description of this screen.  | 
                                                
| 
                                                         Settings > Set Up Device Type Categories  | 
                                                    
                                                         Displays the Set Up Device Type Categories. See Managing device type categories for a description of this screen.  | 
                                                
| 
                                                         Settings > Set Up Engineering Unit Templates  | 
                                                    
                                                         Displays the Set Up Engineering Unit Templates screen. Click Set up engineering templates and select conversions for a description of this screen.  | 
                                                
| 
                                                         Settings > Set Up Trend Definitions  | 
                                                    
                                                         Displays the Set Up Trend Definitions screen. Click for more information.  |