Supported device types and protocols

When you install Power Operation, you are prompted to choose the drivers that you will use. A certain number of generic drivers are installed by default (including PowerLogic device types), and you are not prompted for them. Device types and protocols supported in Power Operation are:

  • Generic MODBUS (includes BCPM and any device, such as a PLC or UPS, that communicates via MODBUS). When adding a controllable device in the Profile Editor, such as a circuit breaker, use the “Controllable Device” driver; otherwise, use the “Generic Power Device” driver. For JBus devices, select Generic JBus Device.
  • Sepam 20, 40, and 80 Range, 2000
  • Masterpact MicroLogic 5P and 6P, A, H
  • Compact NSX (MicrologicV)
  • CM2000
  • CM4000 series
  • PM650
  • PM800 series
  • PM5000 series
  • PM700 series
  • ION protocol devices
  • IEC 61850 protocol devices
  • IEC 870-5-104
  • DNP3
  • BCPMA (branch circuit power meter, full feature support)
  • CSI SER (Cyber Sciences SER)
  • ProTime 100 SER (Monaghan Engineering)