Time synchronization
Current time can be sent to the corresponding device by means of Set Time command or (in case of Sepam) by writing directly to the corresponding registers within the device. In addition to the manual procedure, this process can be scheduled to occur periodically (using Power Operation events).
Non-manual time synchronization causes the Set Time command to be sent automatically, based on a device state or event originating from within the device.
Automatic time synchronization applies only to Micrologic and PM devices and takes place based on the following rules:
- For Micrologic devices, the value of the top-most bit of the register 679 is examined (for both the Circuit Breaker Manager and the Chassis Manager). If the bit is equal to 1, it means that the device is out of sync and needs to be synchronized.
 - For PM devices, an alarm 50700 (“Unary Power Up / Reset”) indicates that the device needs to be synchronized. In addition, bit 6 of register 3055 of the device is examined. If this bit is equal to 1, the device has a real-time clock; so automatic time synchronization should never take place.