Automatic Transfer Switch
An Automatic Transfer Switch (ATS) is an electrical switch that automatically reconnects electric power source from its primary source to a standby source when it senses a failure or outage in the primary source.
The bind properties available for ATS are:
- MainBusColor
 - AuxBusColor
 - CommonBusColor
 - ActiveConditionMain
 - ActiveConditionAux
 
The graphic representation of the default position and the bind properties is explained in the below table:
| Bind Property | Description | Graphic | 
|---|---|---|
| NA | ATS is in default position. | 
                                                         
                                                     | 
                                                
| ActiveConditionAux | ATS is connected to auxiliary power source. | 
                                                         
                                                     | 
                                                
| ActiveConditionMain | ATS is connected to main power source. | 
                                                         
                                                     | 
                                                
- TopBusColor
 - IsTripped
 - IsClosed
 - RkdPos
 - BottomBusColor
 - EarthSwitchClosed