Motor
A motor is an electrical device, which converts electrical energy into mechanical energy, using the principles of electricity and magnetism.
The different types of motors that are supported in the Power Operation are:
- ANSI motor
 - IEC motor
 - AC motor
 - DC motor
 
The bind properties available for ANSI/IEC motors are:
- DestBusColor
 - IsMotorOn
 - SourceBusColor
 
AC/DC motors has only one bind property; BusColor.
The graphic representation of the default position and the bind property is explained in the below table:
| Type | Bind Property | Description | Graphic | 
|---|---|---|---|
| All | NA | Motor is in default position. | 
                                                         
                                                     | 
                                                
| ANSI/IEC motors | IsMotorOn | Motor is On. | 
                                                         
                                                     | 
                                                
| If the motor is Off, the circuit representation looks as shown. | 
                                                         
                                                     | 
                                                ||
| AC/DC motors | BusColor | Sets the bus color. | 
                                                         
                                                     |