Setting up custom tags
Use the Add / Edit Custom Tags window to create, edit, and delete custom tags.
To create custom tags:
- Open the Add / Edit Custom Tags window using one of the following methods:
- At the bottom of the Add / Edit Device Type window, click Add / Edit Custom Tags.
- In Profile Editor, click Settings > Set Up Custom Tags.
- Set up the custom tag using the Add / Edit Custom Tag fields.
The following table describes the Add / Edit Custom Tag fields.
NOTE: See Edit a custom tag and Delete a custom tag for instructions on how to edit or delete custom tags.
NOTE: Starting in Power Operation 2022, item names have an increased importance. They drive binding in web graphics, and determine the availability of those bindings in the Graphics Editor. It is important for tags that will be used in graphics to have item names.
|
Field Name |
Valid Entries |
Comments |
|
Custom Tag Options |
Create New |
Click to begin adding a new tag. |
|
Create From |
Click to begin adding a new tag that is based on an existing custom tag. For example, you might want to change metadata for another custom tag. |
|
|
Edit Existing |
Click to edit the attributes of an existing tag. |
|
|
Delete Existing |
Click to delete a tag (tag cannot be associated with a device type). |
|
|
Tag to Create From Tag to Edit Tag to Delete |
From the drop-down menu, select the tag you want to create from, edit or delete. |
|
|
Delete button |
Live only when Delete Existing is selected. Click to delete the tag. You can only delete custom tags not associated with a device type. |
|
|
Display Associated Device Types |
Click to display device types that are associated with this tag. |
Live only when in Edit mode. Click to list device types that are associated with this custom tag. Note the device types so that you can delete the tag from them (in the Add/Edit Device Type screen) before you delete the tag. See Delete a custom tag for instructions on using this button. |
|
Tag Name |
Type the new tag name; or type the changed name for a tag you are editing. |
Maximum 32 characters; can include any alpha or numeric character, as well underscore (_) and backslash (\). Must begin with either an alpha character of underscore. |
|
Display Name |
Type the name that you want to display when selecting the tag and in other displays. |
You can use this field for additional information on the Add/Edit Custom Tags screen. For example, you could describe the data that it logs. It does not display anywhere else in the system. |
| Item Name | Type the item name for the tag. | Maximum 45 characters; can only include alphanumeric characters. Must begin with a letter. |
|
Group |
Select the group. |
Includes all the real-time groups (such as 100ms, controls, currents) plus onboard alarms, resets, and controls. |
|
Data Type |
Select the data type. |
These are Power Operation tag data types. They affect the logic codes that are available for display in the Edit Address screen. See About logic codes for the data type that matches each logic code. |
|
Eng. Units |
Select the base unit. |
These are the base engineering units for tags; the values come from Engineering Unit Setup. |
|
Ignore Unit Conversion |
Check to cause the system to ignore any conversions that were added for this tag. |
Causes reporting to be according to the base unit, rather than the conversion that was chosen for this tag in the template that is being used. |
|
Add Eng Unit |
Click to open the Add/Edit Units screen, to add a new engineering unit or conversion. |
Provides a quicker means of adding an engineering unit that had been overlooked. |
|
Citect Format |
Select the numerical format. |
This is used for display purposes in Power Operation graphics pages. It determines where the decimal displays. Choose the reporting format, to be used in Power Operation, from ## to #0.#####. For example, if you select #.##, the number 8.12579 would be displayed as 8.12. |
|
Polling Priority |
Low, Normal, or High |
Indicates the level of priority Power Operation uses when reading data from devices.
NOTE: In the address field, a priority of 1 = High, 2 = Medium, 3 = Low. |
|
Alarm On Text |
For onboard alarms only: enter the text for when the alarm is On. |
This text displays on the Create Device Profiles tab for the onboard alarm tag, when it is selected for the device type in the profile. It also displays in the Alarm Log.
|
|
Alarm Off Text |
For onboard alarms only: enter the text for when the alarm is Off. |
|
|
Display ‘Advanced’ filter selections |
Check to display additional filter options in the Real Time Filter and Alarm Filter tabs |
Displays several additional filter options on the two “Filter” tabs. These options will be useful in the future for reporting purposes. |
|
You can include additional filters for either real time filters or alarm filters. Though not currently used, these filters will provide metadata for later reporting. Standard tags have some of these filters selected. A typical usage for these filters might be: when creating a custom tag from an already existing standard tag, you can create matching metadata by using the filters that have been built in to the standard tag. |
||
|
Real Time Filters tab (dropdown lists are expanded when “Display ‘Advanced’ filter selections” is checked) |
||
|
Category Type |
Select a category for this tag. |
This field provides metadata about the tag. It will be used in future reports. |
|
Utility Type |
Select a utility type. |
Metadata for future use in reporting. |
|
Statistical Type |
Select a statistical type. |
Metadata for future use in statistical reporting. |
|
Quantity |
Select a quantity. |
Metadata for future use in statistical reporting. |
|
Alarm Filters tab (dropdown lists are expanded when “Display ‘Advanced’ filter selections” is checked) |
||
|
Categorization |
Select the alarm category |
Used for filtering and sorting alarm data, and metadata for future use in statistical reporting. |
|
Alarm Type |
Select the alarm type. |
Used for filtering and sorting alarm data, and metadata for future use in statistical reporting. |
|
Alarm Group |
Select the group. |
Used for filtering and sorting alarm data, and metadata for future use in statistical reporting. |
|
Subcategorization |
Select a subcategory. |
Used for filtering and sorting alarm data, and metadata for future use in statistical reporting. |
|
Alarm Level |
Select the severity level of the alarm. |
Used for filtering and sorting alarm data, and metadata for future use in statistical reporting. |