System Definition

Use System Definition to set the project display settings.

To set the project display settings:

  1. For Name, click either Create New or Edit Existing.
    1. If you click Create New, enter a project name. Use only alphanumeric characters and underscores.
    2. If you click Edit Existing, choose a project from the list.
  2. Under Resolution, choose the screen resolution that you want for the graphics pages in this project. This should match the resolution of the monitor that will display graphics pages.
  3. Under Style, choose the contrast. Standard uses a white background. High Contrast uses a black background, which makes it easier to view graphics pages.

    NOTE: You can also set high contrast using the parameters in the Power Operation Studio. Open your project in the Power Operation Studio, then click Settings > Parameters. The parameter name is IsHighContrast. 0 = standard; 1 = high contrast.

  4. Click Next.

NOTE: After you click Next, the project is created. You cannot change or delete the project in Project Setup . To change or to delete it, use the Power Operation Studio.