Select Trend Intervals

Use the Select Trend Intervals screen to edit settings for existing trends for specific device profile/tag combinations. To create new trends, see Set Up Trend Intervals.

To change a trend interval, follow these steps:

  1. On the Create Device Profiles tab, choose the device profile, then click the Trend Tags sub-tab.
  2. Locate the tag for which you want to change the trend. Click Edit.
  3. In Select Trend Intervals screen, you can select one or all of the interval options.
  4. Click OK.