Create Device Profiles tab

The Create Device Profiles tab displays all of the tags that are included in each device type profile. It is the starting point for creating/editing device profiles for individual devices. Most of the data on this screen displays for information only; however, to enable waveforms, you need to check the Waveform box (see Enable Waveforms for more information).

The following table describes the fields on this tab. The tags listed assume that Advanced Properties has been checked. Not all elements appear on every sub-tab. Detailed instructions are after the table.

Field Name

Valid Entry

Comments

Tag Groups (left-hand pane)

Click a group to display the groups of tags that have been selected for the chosen device profile.

To associate tags and tag groups with a device type (thus creating a device profile), click Add/Edit.

Device Profile

Choose the device for which you want to view profile details.

Device Profiles are created on the Add/Edit Device Profile screen (click Add/Edit).

Add/Edit button

Click to display the Add/Edit Device Profile screen.

Use that screen to add device profiles and to associate PC-based alarms and trends.

Tag type sub-tabs

 

Click to display the selected tags for each type of tag: real-time, trend, PC-based alarm, onboard alarm, control, or reset.

Organized according to tag groups.

Tag Description

n/a

This is the tag name used when adding the tag.

IEC Tag Name

n/a

This is the IEC 61850-compatible name created when the tag was added.

Waveform

(Onboard Alarm)

Check this box as part of the process of enabling waveform viewing.

You must also set up the alarm and waveform capture in the onboard files of the device. Waveforms will then be viewable in the runtime environment.

Category Type

(Real Time)

n/a

These are real-time filters. They provide metadata to be used in future reporting.

Utility Type

(Real Time)

n/a

Statistical Type

(Real Time)

n/a

Quantity

(Real Time)

n/a

Categorization
(PC Based and Onboard Alarm)

n/a

These are alarm filters. They can be used for filtering and sorting alarm data in the runtime environment. They also provide metadata to be used in future reporting.

Subcategorization

(PC Based and Onboard Alarm)

n/a

Alarm Type

(PC Based and Onboard Alarm)

n/a

Alarm Group

(PC Based and Onboard Alarm)

n/a

Alarm Level

(PC Based and Onboard Alarm)

From the drop-down list, you can edit the alarm level.

If PC-based or onboard alarms are set for this profile, you can change their levels here.

To view profile information:

  1. Select the device profile from the drop-down menu.
  2. Use the tag tabs (such as real-time, trend) to view the tag groups included in this device profile.

To begin adding, editing, or deleting a profile, click Add/Edit.