Power Operation OPC DA

Architecture #1: Simple system without redundancy

The following image illustrates the simplest system that can be configured for a 3rd party application that is consuming or sending OPC information to the Power Operation Server.

NOTE: OPC DA client/server is included and hosted on the Power Operation Server.

 

Architecture #2: OPC DA client/server with Server redundancy

The following image illustrates a redundant Power Operation system that is sending and consuming data from OPC DA to a 3rd party application.

The ability to support the redundant Power Operation architecture depends on the 3rd party application. If the 3rd party application does not have a concept of working with redundant systems, then you should connect to the Primary Server, as pictured. Otherwise you can configure the 3rd party application to connect to both Primary and Secondary Servers.

NOTE: OPC DA client/server is included and hosted on the Power Operation Server.