Installing the ETL Administration Tool
The ETL tool extracts historical data from and transforms it into a format that loads it into Power Monitoring Expert. Install ETL on the machine hosting Advanced Reporting and Dashboards.
Go to the Schneider Electric Community and download the ETL Administration tool.
Install ETL on the machine hosting Advanced Reporting and Dashboards. Install the ETL Administration Tool on the Power Monitoring Expert server using a Windows Administrator account.
To install ETL for PO:
- In Windows Explorer, navigate to \Power Operation with Advanced Reports ETL.
- Copy the PO to PME ETL EXE to the PME server.
- Double-click
SegApps_ETL_PowerSCADA-xxx.exe
.(Where xxx is the build number.)
- Application Language: Select your preferred application language from the drop-down list and click Next.
NOTE: The ETL Administration Tool supports English only.
- Welcome: Review the steps and click Next.
- License Agreement: Read the End User License Agreement and if you accept the terms of the agreement, click I Agree to proceed.
- Setup Type: ETL: Power Operation 2024 can only be installed with the Standalone Server option. Click Next.
- File Destination: Click Next to install the ETL tool to the default location. To select a different location, click the ellipsis button and then select a new location. Click OK.
- Check System: The installer checks the operating system. If a condition affecting installation is detected, the installer notifies you to correct it. When verification is successful, click Next.
- Ready to Configure: A summary of your configuration choices for the installation. Ensure that all items are correct before proceeding.
- Click Install to continue or click Back to move back through the installer and change any items.
The Copy Files screen appears and the ETL files are copied to the system.
- Configure System: The selected configuration settings are applied.
- Click Next.
- Complete: The Complete page appears after the install is successful. Click Installation Log to view details recorded for the installation process.
- Click Close to finish.
After installing the ETL (PO to PME) you will need to allow the ETL to remotely access the Power Operation Server.