Getting started with Power Operation

Power Operation is a suite of tools that lets you develop, design, and deploy SCADA systems. Built on the Plant SCADA platform, Power Operation Studio is the main SCADA development portal. Use Power Operation Studio to:

  • Create, manage, and customize SCADA projects
  • Create and manage I/O devices
  • Design Power Operation Runtime elements
  • Manage user access
  • Open other SCADA productivity tools.

Power Operation is shipped with a project that has example page configuration.

To open Power Operation Studio:

  • Click Start > Schneider Electric > Power Operation Studio
  • OR

  • From the desktop, open the Power Operation folder and then open Power Operation Studio.