Add-ons selection

After you select the Configuration and Development Environment install option from the Core Components page, select the add-ons that you want to include in your installed system. The options are described here:

Project DBF Add-in for Excel

Installs an Add-In for Microsoft Excel. When this Add-In is loaded into Excel, it allows you to browse, open, edit and save Power Operation .dbf files in the correct format. This option can be selected if Microsoft Excel 2007 or above is installed on the computer. Otherwise, it is deselected and disabled.

Power Operation EWS Server

Installs the Power Operation EWS Server. EcoStruxure Web Services (EWS) for Power Operation shares real-time, historical, and alarm data with EcoStruxure™ Building Operations (EBO) and historical data with Power Monitoring Expert (PME).

Power Operation Profile Editor

Installs the Profile Editor. Profile Editor lets you create tags, device types, devices, and projects outside of the Power Operation Studio environment.

OPC Factory Server (OFS)

Installs the OPC Factory Server. OFS is an OPC data access server that may be used to read or write data on devices. For additional information, refer to the OPC Factory Server User Manual which is available in the EcoStruxure™Power Operation Install directory.