Editing a PO to PME ETL job
Edit a PO to PME ETL when you:
- Add a new device in PO
- Edit an existing device name in PO
- Change device logging in a PO device that is mapped to PME.
NOTE: Sources cannot be deleted from Power Monitoring Expert Management Console. To delete PO devices from PME you must contact technical support.
Prerequisites
In order to edit an ETL job, you must know:
- The name of the PO device you want to map. (If you are adding a new PO device to the ETL job.)
- The name of the mapped PME source. (If you are editing a PO device name or measurement in the ETL job.)
To edit a PO to PME ETL job:
- Open ETL (PO to PME).
- (Optional) If the ETL job that you want to edit is registered to run as a service, select the job you want to stop and select Control and then Stop to stop the service. Then select OK to close the Job Control page.
- From the list of jobs, select the job that you want to edit and then select Edit.
- In the Mappings pane, select Load Sources.
The ETL tool displays how many new records were added. The newly named PO source device and measurement appears in the grid in the Source Tag column, along with a suggested Target Device.
- Filter the list of devices to locate the PO Source Tag row containing the PO source you want to map.
See Tips for working with mappings for details on how to filter loaded sources.
- Review the Target Device value in the same row.
The Target Device value is the PME source under which the PO data will be loaded.
-
If the Target Device name and measurement matches the expected name in PME, select Include Selected Mappings. If the Target Device or Target Measurement does not match the expected value, edit the Target Device field and then select Include Selected Mappings
NOTE: If you want to log data for the PO device continuously under the same PME device as it did prior to the PO tag renaming, map the new PO tag to the same PME target device. This may be useful when viewing historical data in PME over the time span of the PO tag renaming.
- Select Apply.