Configuring a thermal monitoring device profile
To create a thermal monitoring device profile:
NOTE: By default, a Switchgear Monitoring Device has Cubicle 1, Transformer 1, and Location 1 tags in the profile. If you only need those tags, skip to step 10.
- Open the Profile Editor and select the Create Device Profiles tab.
- In the Device Profile drop-down, select Switchgear Monitoring Device and select OK.
- Select Add/Edit.
- In the Add/Edit Device Profile window, select Create From and select Next.
NOTE: Make sure Switchgear Monitoring Device is still selected in the Device Profile to Create From drop-down.
- Enter a new name for the device profile, for example SMD Standard, and select Next.
- Confirm Switchgear Monitoring Device appears in the Selected Devices section, and then select Next.
-
In the Device Types Tags section, select the Cubicle, Transformer, and Location tags you need for the SMD, and select the
to add them to the device profile.
NOTE: By default, a Switchgear Monitoring Device has Cubicle 1, Transformer 1, and Location 1 tags in the profile. If you only need those tags, select Cancel and skip to step 10.
- Select all the tags you need and select Next.
- Select Close Wizard and select Finish.
NOTE: Select any SMD trending tags you need in this window. By default, no tags are selected for PC Based or Trend.
- Select the Set Up Projects tab and select Add/Edit.
- Select Create New, then select
, select your project, and select OK.
- In the Device Profiles section, select the device profile you created and select
to move it to the Selected Device Profiles section.
NOTE: If you skipped directly to step 10, select Switchgear Monitoring Device.
- Select Save & Exit.
- Select Export Project to export the new profile to the Power Operation project.