Configuration prerequisites

  • Review the system development process provided in this help.
  • Gather the supporting documents that you may need.
  • Create a system architecture drawing, including the servers, devices, and all connectivity. Define the IP addressing for each gateway and device.
  • Order the appropriate equipment, including computers, software, and system devices.
  • Confirm that all devices that will communicate through this system are set up and properly addressed.
  • Have a copy of the Example.CSV file for adding devices to the system. You will use this file if you need to manually add multiple devices to your project.
  • Set up the Server and Client computers that you need for your system.
  • Confirm that the IT team has opened the appropriate firewall ports. See the Power Operation with Advanced Reporting and Dashboards – IT Guide for details.
  • Confirm that all license keys have been purchased and are ready to be installed.