Printing the .CSV file
For each device type, device profile, or project, you can create and print a CSV file that includes the following data:
|
Type of File |
Data Included |
|
Device Type |
tag descriptions, IEC tag names, type, and address |
|
Device Profile |
tag descriptions, IEC tag names |
|
Project |
data profiles and custom tag names included in the project |
To create and print the CSV file:
- Display the device type, profile, or project for which you want the file. For example, to create a CSV file for the Sepam 42 Full device profile, select the Create Device Profiles tab and choose Sepam S42 Full from the drop-down list.
- Select File > Create CSV File.
- In the Save As window, choose a location for the file and optionally rename it. Select Save.
The file is created in the location you specified.
- View and print the file in Microsoft Excel.