Edit driver parameters

Certain IEC 61850 devices may have driver parameters associated with them. You can edit the datasets and report control blocks that will then be exported to Power Operation.

To begin editing driver parameters: from the Create Device Profiles tab, select the Parameters sub-tab.

To begin editing datasets, select Edit in the DataSets line. Follow instructions in Managing IEC 61850 datasets for help.

To begin editing report control blocks, select Edit in the Report Control Blocks line. Follow instructions in Edit IEC 61850 Report control blocks for help.