Enabling and testing notification delivery
After you have configured all the notification components, choose the delivery methods that Notifications Settings will use to notify people if an alarm occurs.
Prerequisites:
- Email and SMS setup is complete
- Email and SMS templates are defined
- The notification has at least 1 alarm filter
- The notification has at least 1 recipient
To enable notification delivery:
- In the Delivery section of the Notifications pane, select the delivery methods you want to use to notify people.
- For each delivery method you enable, select Test to make sure the it works as expected.
- Select Save.