Customize tag names

From the Set Up Project tab, select the Customize Tag Names sub-tab.

You can add a custom name for any tag in the system, predefined and custom tags. The customized name will be used anywhere the original name would be used, but only for the project that is selected in the drop-down menu. When you use the Export option, it will be used by the I/O Device Manager.