Creating virtual datapoints
In Profile Studio, create formulas using datapoints as inputs. These are called virtual datapoints.
NOTE: This feature is only available for an EPAS system.
To create virtual datapoints:
SPS2DPS is a DPS type created from an SPS.
- Select a location in the Navigation pane below the root node.
- In the Virtual datapoints tab, right-click and choose one of the following from the context menu:
- SPS
- SPC
- DPS
- DPC
- MPS
- MV
- SPS2DPS
The virtual datapoint appears in the Virtual datapoints tab.
To define virtual datapoint inputs and formulas:
- Select your virtual datapoint.
- In the Configuration pane Virtual datapoints tab, click the Edit inputs button.
- In the Information dialog, click OK.
- In the Datapoints tab, select a datapoint with an associated profile (in black).
- Select the
button. The datapoint is associated with the virtual datapoint you created.
- Select the Edit formula button.
- In the Virtual datapoint editor, define a formula to calculate the virtual datapoint's value from the associated datapoint.
- On the Signal quality drop-down list, select one of the following:
- AlwaysValid: The formula is always valid.
- ValidIfAllSignalsAreValid: The formula is valid when all signals (input) are valid.
- ValidIfOneSignalIsValid: The formula is valid when one of the signals (input) is valid.
- Select OK.