Add Redundant NetworkTagsDev and zOL Devices
For systems with redundant I/O devices, you will need to create redundant NetworkTagsDev and a zOL device.
- Open the I/O Device Manager.
 - Select Create an I/O Device in the project.
 - Under System Devices, choose Cluster Setup.
 - Accept the default device/equipment names.
 - Check Supports Redundancy.
 - Set the primary server to one of the available I/O servers.
 - Set the standby server to one of the I/O servers on a different network address.
 - Allow to finish and select Add/update/remove more devices.
 - Select Create an I/O Device in the project.
 - From System Devices choose OneLine Device Setup.
 - Accept the default device/equipment names.
 - Finish and close I/O Device Manager.