Compile the project

After you install the software and create the project—along with clusters, network addresses, and servers—compile the project. You will also need to compile your project periodically during system setup.

Pack your project before you compile. In Power Operation Studio, click the Projects activity, click Pack.

In Power Operation Studio, click Compile . If you are promoted to save your changes, click Save.

If there are errors or warnings after the project is compiled:

  1. At each error, click GoTo, which opens the location where the error occurred.
  2. Using the information in the error message, correct the error.
  3. After all errors are addressed, re-compile to verify that the errors are removed.

    For additional information, click Help at the error screen.