Backing up a project
To back up a Power Operation project file:
- In Power Operation Studio, select Projects
.
- Select Backup.
- From the Name drop down, choose the project you want to back up.
- (Optional) Select Select all included projects.
- Select Browse and then browse to the location where you want to store the project backup file.
- In the Options area, select Save configuration files. This saves the citect.ini file.
- Select OK.
The backup CTZ file is written to the location that you choose during backup. This is a Citect Zip file; you can open it with WinZip.
NOTE: To back up a Profile Editor project file, see Profile Editor export.