Back up the Power Operation Studio project
Back up your Power Operation project. You will subsequently restore the project on the Secondary Server. (To back up the Profile Editor, use the Export feature on the Projects tab.)
To back up a Power Operation Studio project file:
- In Power Operation Studio: Select Projects, and then select Backup.
- In the Backup Project window, select the project you want to back up.
- Browse to the location where you want to store the backup file.
- In the Options box, select Save configuration files. This saves the citect.ini file. Also, select Save sub-directories and Use Compression.
- Select OK.
- Backup the citect.ini file from the Primary Server for later use in merging settings into the Secondary Server's citect.ini file.
The backup CTZ (Citect ZIP) file is written to the location that you chose during backup. You can open it with WinZip.