Restore the Power Operation Studio project

To restore the project:

  1. In Power Operation Studio, select Projects .
  2. Select the Backup drop down and then select Restore.
  3. Beside the Backup file text field, select Browse, and then browse to the location of the project file you will use to restore.
  4. (Optional) Select Select all included projects.
  5. In the To area, select Current Project.
  6. In the Options area:
    1. Select Configuration files to restore backed up INI files and the TimeSyncConfig.xml file (used to store time synchronization settings).
    2. Select Select sub-directories. The sub-directories included in the earlier backup will be listed.
  7. Select OK.