Default CAE security settings

The following table defines the default security settings for the Cybersecurity Admin Expert (CAE) tool:

Area Setting Default
User accounts Security administrator username and password (access to CAE)

Username: SecurityAdmin
Password: AAAAAAAA

Security auditor username and password (access to CAE) Username: DefaultSecAud
Password: AAAAAAAA
Default arrow password for all default user accounts

Enter this password twice, starting from the left arrow and go clockwise:

  1. Left

  2. Up

  3. Right

  4. Down

Preconfigured user accounts (no access to CAE) DefaultEngineer, DefaultInstaller, DefaultOperator DefaultRbacMnt, DefaultSecAud, DefaultViewer, SecurityAdmin
Models Models Disabled
Security Settings > User Accounts Minimum activity period (min) 15 mins.
Password complexity None
Number of previous passwords that cannot be reused 3
Activate 'Local Default Access' Yes. VIEWER by default.
Allow user account locking 15 mins.
Maximum login attempts Yes
Password attempts timer (min.) 5
Automatic user account locking Enabled
User account lockout duration (s) 240 seconds
Logs Log and monitoring standard BDEW
Server port 601
SYSLOG parameters server port 601
Security Banners Banner on device front panel displays None
Authentication Configuration Authentication mode Local
Default role for centralized authentication Viewer
Centralized authentication timeout duration (s) 5 seconds
Centralized authentication protocol None