Using the Security Viewer Filter

To filter for the information that displays in the security viewer log, select Filter (in the upper left corner of the screen). The Security View Filter screen displays.

The following table describes the Security View Filter settings:

Filter option Description: Display alarms for:
Basic Filter box:

Start Date/End Date

Choosing only a start date displays alarms from that date to the current date.
Choosing only an end date displays alarms for the past year up to that date.
For example, to display alarms only for today’s date, enter only a start date.

Start Time/End Time

Choosing only a beginning time displays alarms from that time through the end of the day (23:59:59 or 11:59:59 p.m.).
Choosing only an ending time from the start of the day (00:00:00 or 12:00:00 a.m.) through the time selected.

Cluster

This is a single cluster, which was added when setting up the project (listed in Project Editor > Servers > Clusters)

Area

Area (Between 0 and 255). See Alarm SOE fields in the Plant SCADA help file ( ..\Program Files (x86)\Schneider Electric\Power Operation\v2024\bin\Help\SCADA Help).

Classification

The class of the event. See Alarm SOE fields in the Plant SCADA help file ( ..\Program Files (x86)\Schneider Electric\Power Operation\v2024\bin\Help\SCADA Help).

Operator

The user ID of the person who has logged on Power Operation.

Message

This comes from the Message field in the Alarm Log.

Custom Filter

There are eight custom filters, which can be assigned by the customer in each alarm. A group of alarms in a specific location could have the same name in CUSTOM8 so that custom filtering can be easily applied.

Custom8 has a default assignment of “Equipment.” To change custom filter assignments, use the AlarmFormat parameter (Project Editor > System > Parameters). This is the only means available for filtering on a custom field. When viewing the log, you can use the new custom filter by typing it into the Custom Filter field.