Using single sign-on and passwords

With single sign-on (SSO), you associate a Citect user with a Power Operation username and password or a Power Monitoring Expert username and password. This allows the Citect user to access external applications, such as Dashboards, using an SSO user password from Power Monitoring Expert.

NOTE: SSO only works with Client Access.

For information on using trusted certificates, see Certificate requirements for webpages.

For information on using SSO with the Advanced Reporting and Dashboards Module, see Adding Advanced Reporting and Dashboards into Web Applications.

Topics in this section: