Activating a Binding with a Dynamic Update Attribute

You edit the DynamicUpdate attribute to improve the performance when loading a graphic. By default, the dynamic updates are enabled, that is, the value connected to the Bind element of the graphic is updated when the graphic is opened.

For more information, see the Dynamic Updates section.

To activate a binding with a dynamic update attribute:

In Graphics Editor, in the Objects pane, select the Bind element for which you want to edit the DynamicUpdates attribute.

In the Properties pane, in the Behavior area, select the DynamicUpdates attribute and select Enable or Disable depending on whether or not you want the graphic to subscribe to the value connected to the Bind element when the graphic is opened.