Editing an Arc or Pie
You edit the start and sweep vertexes of an arc or pie to change its angle.
To edit an arc or pie:
- In Graphics Editor, in the work area, double-click anywhere on the arc to display the vertexes.
- Select the vertex you want to edit and drag it to a new position.
NOTE: You can extend the angle handle to increase the precision. This does not affect the arc in other ways. If you press the Shift key while moving the cursor, the angle changes in steps of 7.5°, somewhat depending on how much you extend the handle.
- Click outside the arc to finish.