Snippets Overview

Snippets are standardized, predefined functions for defined use. Snippets typically represent a feature in a live system. Snippets are located in dedicated libraries and are displayed in the Graphic Editor Snippets pane. Blink, which starts and stops a blink animation, is an example of a snippet.

By default, the Graphics Editor uses two dedicated folders, containing sub folders, for Components and Snippets. The folders are installed with the software. If your computer runs on Windows 7, Windows 8.1, or Windows 10, the components and snippets folders have the following paths:

...\ProgramData\Schneider Electric\Power Operation\Applications\Graphics\SnippetLibraries\Snippets\Basic Snippets

The sub folders are displayed as categories in the Components and Snippets panes.

Libraries can be located anywhere on the local disk. You can show and hide categories from a selected library. You can add categories.