Drawing an Arc or Pie
Arc
Use the Graphics Editor Arc tool to draw an arc, that is, a part of the periphery of an ellipse, or a circle.
The arc is defined by a center point, a radius X, a radius Y, a start angle, and a sweep angle. The start angle is the angle between the X-axis and the start of the arc. The sweep angle can lie in the interval ±(0° – 360°).
Pie
Use the Graphics Editor Pie tool to draw a pie, that is, an area enclosed by two radii of a circle and their intercepted arc.
The pie is defined by a radius X, a radius Y, a start angle, and a sweep angle. The start angle is the angle between the X-axis and the start of the arc. The sweep angle can lie in the interval ±(0° – 360°).
A pie is similar to an arc, but includes the two radii and the area within.
Arc or Pie
Use Arc or Pie to draw a curve-like segment, but with specified start and end points. The initial sweep angle is always 90°. The orientation of the 90° arc or pie corresponds to the position of the end point, related to the start point.
To draw an arc or pie:
- In Graphics Editor, in the Layers pane, select the layer where you want to draw the arc or pie.
- On the Drawing toolbar, select Arc. The cursor will change into a crosshair pointer.
- In the work area, drag the pointer from where you want to start the arc or pie to where you want it to end.
- On the Drawing toolbar, select Select.
- In the Properties pane, in the Name box, type the name of the arc or pie.
NOTE: You only need to name the drawing object if you will be binding the object. Naming the object now will help you identify the object later.
- On the Options toolbar, or in the Properties pane, adjust the appearance of the arc or pie.
- On the File menu, select Save.