Log in with YubiKey

Use this procedure to log in to Power Operation using a YubiKey and a one-time password.

Prerequisites:

The YubiKey is programmed and associated with a user in Power Operation, and the YubiKey is enabled.

To log into the system using YubiKey:

  1. Insert the programmed YubiKey into a USB port of the Power Operation server.
  2. Launch Power Operation Runtime, or access runtime using a remote Web Client.
  3. Run the project you want to view.
  4. In the upper right corner of the Startup screen, click Login.
  5. In the Power Operation Studio login screen, enter your name and password and then click OK.
  6. The One-time Password screen appears.

  7. Press the button on the YubiKey.

The one-time password is generated. The key and software communicate behind the scenes to verify the uniqueness of the one-time password and to click OK.

You can start using Power Operation Runtime.