Alarms configuration

Use Alarms to view incidents, alarms and events. You access the information in Alarms through views which are saved in the View Library. Power Operation comes with a number of pre-configured System Views. These system views cannot be deleted or modified, but you can create additional views and customize them to meet your needs.

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

warning

unintended equipment operation

Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action.
Do not use the software to control time-critical functions.
Do not use the software to control remote equipment without proper access control and status feedback.

Failure to follow these instructions can result in death or serious injury, or equipment damage.

TIP: Open Alarms from the ALARMS link in the Web Applications banner.

Topics in this section: