Alarm Views
Use the Alarm View settings to:
- Change the number of items that are displayed in the alarms viewer.
- Change the priority classifications for alarms and incidents.
- Customize the behavior of the alarm annunciator with these settings.
- Customize the display of Load Impact events in Alarm and Incident views.
To change the number of Incidents, Alarms, and Events displayed in the Alarm Viewer:
- Open Power Operation.
- SETTINGS > Alarms > Alarm Views.
-
Enter values for:
- Maximum Number of Incidents Displayed: changes the maximum items displayed in the Recent Incidents view.
- Maximum Number of Alarms Displayed: changes the maximum items displayed in All Alarms and Recent Alarms views.
- Maximum Number of Events Displayed: changes the maximum items displayed in the Recent Events view.
- Select Save.
To change the Alarm Viewer update interval:
- Under Display Settings, select the Update Interval.
- Select Save to apply the changed settings.
To turn the Alarm Annunciator on or off:
- Under Annunciator, turn Enable on or off.
When the Annunciator is turned off, it is not visible in the Web Applications banner.
- Select Save to apply the changed settings.
To change what type of state counts are shown in the Alarm Annunciator:
- Under Annunciator, select the state type for Show counts for.
- Select Save to apply the changed settings.
To change the Alarm priorities that are shown in the Alarm Annunciator:
- Under Priority Classification, select or clear the Visible in Annunciator check boxes for the Alarm priorities you want to include or exclude from the Annunciator.
- Select Save to apply the changed settings.
To change for which Alarm priorities an Alarm notification sound is played:
- Under Priority Classification, select or clear the Audible in Annunciator check boxes for the Alarm priorities you want a notification sound to be played for or not.
- Select Save to apply the changed settings.
To change the sound that is played for Alarm notification:
- Under Annunciator, select Select Sound File.
- In Select Audio File, select the sound you want.
NOTE: Only
.mp3
and.wav
file formats are accepted.Or, if the sound is not in the Media Library,
- Select Upload Audio File and either choose a sound file available on your system by clicking Choose Files, or drag a sound file into the application area.
- Select Finish to add it to the Media Library.
- Select OK to complete your sound selection.
- Select Save to apply the changed settings.
To change the Alarm Annunciator update interval:
- Under Annunciator, select the Update Interval.
- Select Save to apply the changed settings.
To change the display color and Alarm priority ranges for the Alarm Viewer:
- Under Priority Classification, set the Color and Start values for the different alarm priorities. The End values are adjusted automatically.
- Select Save to apply the changed settings.
To change the display of Load Impact events in Alarm and Incident views:
- Under Load Impact Display, select or clear the check boxes for the options you want or not.
- Select Save to apply the changed settings.