System Theme
Use the system theme settings to:
- Choose the Default theme or a User Defined theme
- Specify if you want to display the vendor logo in the top right corner of the Web Applications window.
- Change the image and text that is displayed in the top left corner of the Web Applications window.
- Choose a theme color for the borders and other elements of the user interface. You can enable high contrast mode which uses a dark background color for the application.
- Choose the location of the library panel to be on the right or left side of the user interface.
- Specify if you want to use compact mode navigation.
NOTE: Compact navigation replaces the main navigation bar at the top of the Web Applications user interface with an options button
. The options button is displayed at the top left corner of the banner. When you select the button, the navigation links to the different Web applications are shown. Compact mode is used for small displays, such as on mobile devices. The Web Applications user interfaces switches to compact mode automatically when the browser size is reduced below a certain size. Turning on the Always use compact mode for Navigation setting forces this mode regardless of browser size.
- Set the colors for the waveform and bust data plots.
- Reset the theme to system defaults.
To select the theme to be default or user defined:
- Under General Theme, select Default Theme or select User Defined.
NOTE: With the Default Theme all color, image, and logo options are set to the factory defaults. You can change the location of the navigation panel, choose to always use compact mode, and you can customize the colors for the waveform and burst data plots.
- Select Save to apply the changed settings.
To specify the display of the vendor logo:
- Under General Theme, select User Defined.
- Turn on Show Vendor logo to display the logo or turn off Show Vendor logo to hide the logo, in the top right corner of the Web Applications window.
- Select Save to apply the changed settings.
To change the top left logo and text:
- Under General Theme, select User Defined.
- Under Image, select Select.
- In Select Image, select the image you want, or if the image is not in the Image Library,
- Select Upload Image and either choose an image file available on your system by clicking Choose Files or drag an image file into the application area.
- Select Finish to add it to the Image Library.
-
Select OK to complete your image selection.
The image file name is shown under Image. The image is updated on the banner when you save your settings. You can use GIF, JPG, JPEG, or PNG image formats. The maximum file size is 2MB. Images are automatically resized to fit the logo area on the banner.
- Use the Text field to change the text beside the logo in the banner. The text is updated when you save your settings.
- Select Save to apply the changed settings.
To change the theme color:
- Under General Theme, select User Defined.
-
Under Theme Color, select from several preset color themes or create your own using the color selector that opens when you select the color theme icon
on the right. When you select a preset color, it is temporarily applied to the interface to show you the effect of the change.
TIP: Enable high contrast mode to create a dark mode type theme with dark backgrounds.
- Select Save to apply the changed settings.
To choose the location of the library panel:
- Under Navigation, select Left or Right.
- Select Save to apply the changed settings.
To specify the use of compact mode navigation:
- Under Navigation, turn on Always use compact mode for Navigation.
- Select Save to apply the changed settings.
To change the color settings for Waveform and Burst Data:
- Under Waveform and Burst Data, set the color that is used to display the different measurement types.
NOTE: Select Reset to Default to set the colors to the system default.
- Select Save to apply the changed settings.
To reset the theme to the system defaults:
- Select Default Theme.
- Select Save to apply the changed settings.