Trends
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
warning
unintended equipment operation
● | Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action. |
● | Do not use the software to control time-critical functions. |
● | Do not use the software to control remote equipment without proper access control and status feedback. |
Failure to follow these instructions can result in death or serious injury, or equipment damage.
![]() |
||||||||||||||||||||||||
|
![]() |
||||||||||||||||||||||||
|
TIP: You can open the Trends application from the TRENDS link in the Web Applications banner.
Time display
See Time Display in Web Applications for information on how time is displayed in a system where the monitoring devices, the Power Operation/Web server, and the Web client (browser) are located in different time zones.
For information on how use the Trends application, see Trends UI.
For information on how to configure Trends, see Trends configuration.