Default Genie Library
The genie library includes a number of general genies for objects such as motors and pumps. There are also genies that are specific to Power Operation. These genies use a particular naming convention, which is described in the table below. In the Power Operation library, each genie name begins with “pls,” and is followed by a description of the type of genie according to this table:
| 
                                                         first  | 
                                                    
                                                         second  | 
                                                    
                                                         third  | 
                                                    
                                                         fourth  | 
                                                
| 
                                                         pls indicates Power Operation library  | 
                                                    
                                                         alarm = alarm  | 
                                                    
                                                         base = primitive genies  | 
                                                    
                                                         1 = small  | 
                                                
| 
                                                         ansi = ANSI style  | 
                                                    
                                                         cb = circuit breaker  | 
                                                    
                                                         2 = large  | 
                                                |
| 
                                                         display = equipment details  | 
                                                    
                                                         sw = switchgear  | 
                                                    
                                                         
  | 
                                                |
| 
                                                         gen = generic  | 
                                                    
                                                         cmd = control genies  | 
                                                    
                                                         
  | 
                                                |
| 
                                                         iec = IEC style  | 
                                                    
                                                         eq = equipment (devices)  | 
                                                    
                                                         
  | 
                                                |
| 
                                                         style = navigation  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                |
| 
                                                         
  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                
Additionally, the actual genies have abbreviated names. When you highlight a genie name, the abbreviation displays above the top row of genie icons.
The following tables list and define the individual genies in each of the Power Operation libraries.
PLS_ALARM
This library includes genies that provide functionality to alarm displays.
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         Field  | 
                                                    
                                                         data portion of an alarm row  | 
                                                
| 
                                                         Row  | 
                                                    
                                                         a genie with a collection of fields  | 
                                                
| 
                                                         Selector  | 
                                                    
                                                         for column resizing  | 
                                                
| 
                                                         Setpoint  | 
                                                    
                                                         a setpoint row  | 
                                                
PLS_ANSI_BASE_1 / PLS_ANSI_BASE_2
These libraries include a variety of base symbols used to created genies for ANSI equipment.
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         sl_battery_gen  | 
                                                    
                                                         single-cell battery  | 
                                                
| 
                                                         sl_battery_multi  | 
                                                    
                                                         multiple-cell battery  | 
                                                
| 
                                                         sl_capacitor  | 
                                                    
                                                         capacitor  | 
                                                
| 
                                                         sl_capacitor_vari  | 
                                                    
                                                         variable capacitor  | 
                                                
| 
                                                         SL_Closed_HV  | 
                                                    
                                                         closed circuit breaker position  | 
                                                
| 
                                                         sl_closed_knife  | 
                                                    
                                                         closed knife switch  | 
                                                
| 
                                                         sl_closed_lv  | 
                                                    
                                                         closed low-voltage circuit breaker  | 
                                                
| 
                                                         sl_conductive_path_1  | 
                                                    
                                                         conductive path 1  | 
                                                
| 
                                                         sl_conductive_path_2  | 
                                                    
                                                         conductive path 2  | 
                                                
| 
                                                         sl_conductive_path_3  | 
                                                    
                                                         conductive path 3  | 
                                                
| 
                                                         sl_conductor_junction  | 
                                                    
                                                         conductor junction  | 
                                                
| 
                                                         sl_contact_nc_closed  | 
                                                    
                                                         contact break, closed  | 
                                                
| 
                                                         sl_contact_nc_open  | 
                                                    
                                                         contact break, open  | 
                                                
| 
                                                         sl_contact_no_closed  | 
                                                    
                                                         contact make, closed  | 
                                                
| 
                                                         sl_contact_no_open  | 
                                                    
                                                         contact make, open  | 
                                                
| 
                                                         sl_contact_term  | 
                                                    
                                                         contact terminal  | 
                                                
| 
                                                         sl_ct  | 
                                                    
                                                         current transformer  | 
                                                
| 
                                                         sl_in_cb_rack  | 
                                                    
                                                         incoming, circuit breaker racked out, plug  | 
                                                
| 
                                                         SL_In_Rack  | 
                                                    
                                                         incoming, circuit breaker racked out, socket  | 
                                                
| 
                                                         sl_in_sw_head  | 
                                                    
                                                         incoming switch head  | 
                                                
| 
                                                         sl_inductor  | 
                                                    
                                                         inductor  | 
                                                
| 
                                                         sl_inductor_adjust  | 
                                                    
                                                         adjustable inductor  | 
                                                
| 
                                                         sl_inductor_gen  | 
                                                    
                                                         general inductor  | 
                                                
| 
                                                         sl_inductor_magcore  | 
                                                    
                                                         magnetic core inductor  | 
                                                
| 
                                                         sl_inductor_vari  | 
                                                    
                                                         variable inductor  | 
                                                
| 
                                                         sl_open  | 
                                                    
                                                         open symbol  | 
                                                
| 
                                                         sl_open_fuse_sw  | 
                                                    
                                                         open isolating fuse-switch  | 
                                                
| 
                                                         SL_Open_HV  | 
                                                    
                                                         open high-voltage circuit breaker  | 
                                                
| 
                                                         sl_open_knife  | 
                                                    
                                                         open knife-type switch  | 
                                                
| 
                                                         SL_Open_LV  | 
                                                    
                                                         open low-voltage circuit breaker  | 
                                                
| 
                                                         sl_out_cb_rack  | 
                                                    
                                                         outgoing, circuit breaker racked out, plug  | 
                                                
| 
                                                         SL_Out_Rack  | 
                                                    
                                                         outgoing, circuit breaker racked out, socket  | 
                                                
| 
                                                         sl_pb_break  | 
                                                    
                                                         push-button, break  | 
                                                
| 
                                                         sl_pb_make  | 
                                                    
                                                         push-button, make  | 
                                                
| 
                                                         sl_pb_term  | 
                                                    
                                                         push-button, terminal  | 
                                                
| 
                                                         sl_pt  | 
                                                    
                                                         potential transformer  | 
                                                
| 
                                                         sl_relay  | 
                                                    
                                                         relay  | 
                                                
| 
                                                         sl_resistor  | 
                                                    
                                                         resistor  | 
                                                
| 
                                                         sl_resistor_adjust  | 
                                                    
                                                         adjustable resistor  | 
                                                
| 
                                                         sl_resistor_vari  | 
                                                    
                                                         variable resistor  | 
                                                
| 
                                                         sl_separable_con_closed  | 
                                                    
                                                         separable connector, closed  | 
                                                
| 
                                                         sl_separable_con_open  | 
                                                    
                                                         separable connector, open  | 
                                                
| 
                                                         sl_separable_con_plug  | 
                                                    
                                                         separable connector plug  | 
                                                
| 
                                                         sl_separable_con_socket  | 
                                                    
                                                         separable connector socket  | 
                                                
PLS_ANSI_CB_1 / PLS_ANSI_CB_2
These libraries include genies for ANSI-type high-voltage and low-voltage drawout circuit breakers.
1 = small size
2 = large size
Additional definitions:
| 
                                                         bus  | 
                                                    
                                                         =  | 
                                                    
                                                         busway  | 
                                                
| 
                                                         cb  | 
                                                    
                                                         =  | 
                                                    
                                                         circuit breaker  | 
                                                
| 
                                                         
  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                
| 
                                                         hv  | 
                                                    
                                                         =  | 
                                                    
                                                         high voltage  | 
                                                
| 
                                                         lv  | 
                                                    
                                                         =  | 
                                                    
                                                         low voltage  | 
                                                
| 
                                                         
  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                
| 
                                                         dr  | 
                                                    
                                                         =  | 
                                                    
                                                         drawout  | 
                                                
| 
                                                         nd  | 
                                                    
                                                         =  | 
                                                    
                                                         non-drawout  | 
                                                
| 
                                                         
  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                
| 
                                                         fd  | 
                                                    
                                                         =  | 
                                                    
                                                         earth at bottom (feeder)  | 
                                                
| 
                                                         inc  | 
                                                    
                                                         =  | 
                                                    
                                                         earth at top (incomer)  | 
                                                
| 
                                                         nes  | 
                                                    
                                                         =  | 
                                                    
                                                         no earth  | 
                                                
| 
                                                         
  | 
                                                    
                                                         
  | 
                                                    
                                                         
  | 
                                                
| 
                                                         nc  | 
                                                    
                                                         =  | 
                                                    
                                                         not remote control  | 
                                                
| 
                                                         c  | 
                                                    
                                                         =  | 
                                                    
                                                         remote control  | 
                                                
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         hv_cb_bus_dr_c  | 
                                                    
                                                         high-voltage drawout circuit breaker, remote control  | 
                                                
| 
                                                         hv_cb_bus_dr_nc  | 
                                                    
                                                         high-voltage drawout circuit breaker, not remote  | 
                                                
| 
                                                         hv_cb_bus_nd_c  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, not remote  | 
                                                
| 
                                                         hv_cb_bus_nd_nc  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, not remote  | 
                                                
| 
                                                         hv_cb_fd_dr_c  | 
                                                    
                                                         high-voltage, drawout circuit breaker, remote control, with earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_dr_nc  | 
                                                    
                                                         high-voltage, drawout circuit breaker, no remote control, with earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_nd_c  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, remote control, with earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_nd_nc  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, no remote control, with earth at bottom  | 
                                                
| 
                                                         hv_cb_inc_dr_c  | 
                                                    
                                                         high-voltage, drawout circuit breaker, remote control, with earth at top  | 
                                                
| 
                                                         hv_cb_inc_dr_nc  | 
                                                    
                                                         high-voltage, drawout circuit breaker, no remote control, with earth at top  | 
                                                
| 
                                                         hv_cb_inc_nd_c  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, remote control, with earth at top  | 
                                                
| 
                                                         hv_cb_inc_nd_nc  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, no remote control, with earth at top  | 
                                                
| 
                                                         hv_cb_nes_dr_c  | 
                                                    
                                                         high-voltage drawout circuit breaker, remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_dr_nc  | 
                                                    
                                                         high-voltage drawout circuit breaker, no remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_nd_c  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_nd_nc  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, no remote control, no earth  | 
                                                
| 
                                                         lv_cb_bus_dr_c  | 
                                                    
                                                         low-voltage drawout circuit breaker, remote control, busbar-type with earth at bottom  | 
                                                
| 
                                                         lv_cb_bus_dr_nc  | 
                                                    
                                                         low-voltage drawout circuit breaker, no remote control, busbar-type with earth at bottom  | 
                                                
| 
                                                         lv_cb_bus_nd_c  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, remote control, busbar-type with earth at bottom  | 
                                                
| 
                                                         lv_cb_bus_nd_nc  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, no remote control, busbar-type with earth at bottom  | 
                                                
| 
                                                         lv_cb_fd_dr_c  | 
                                                    
                                                         low-voltage drawout circuit breaker, remote control, earth on load side (bottom of drawing)  | 
                                                
| 
                                                         lv_cb_fd_dr_nc  | 
                                                    
                                                         low-voltage drawout circuit breaker, no remote control, earth on load side (bottom of drawing)  | 
                                                
| 
                                                         lv_cb_fd_nd_c  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, remote control, earth on load side (bottom of drawing)  | 
                                                
| 
                                                         lv_cb_fd_nd_nc  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, no remote control, earth on load side (bottom of drawing)  | 
                                                
| 
                                                         lv_cb_inc_dr_c  | 
                                                    
                                                         low-voltage drawout circuit breaker, remote control, earth on feeder (top of drawing)  | 
                                                
| 
                                                         lv_cb_inc_dr_nc  | 
                                                    
                                                         low-voltage drawout circuit breaker, no remote control, earth on feeder (top of drawing)  | 
                                                
| 
                                                         lv_cb_inc_nd_c  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, remote control, earth on feeder (top of drawing)  | 
                                                
| 
                                                         lv_cb_inc_nd_nc  | 
                                                    
                                                         low-voltage non-drawout circuit breaker, no remote control, earth on feeder (top of drawing)  | 
                                                
| 
                                                         lv_cb_nes_dr_c  | 
                                                    
                                                         low voltage drawout circuit breaker, no earth, remote control  | 
                                                
| 
                                                         lv_cb_nes_dr_nc  | 
                                                    
                                                         low voltage drawout circuit breaker, no earth, no remote control  | 
                                                
| 
                                                         lv_cb_nes_nd_c  | 
                                                    
                                                         low voltage non-drawout circuit breaker, no earth, remote control  | 
                                                
| 
                                                         lb_cb_nes_nd_nc  | 
                                                    
                                                         low voltage non-drawout circuit breaker, no earth, no remote control  | 
                                                
PLS_ANSI_SW_1 / PLS_ANSI_SW_2
These libraries include ANSI-style switches:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         sw_fused  | 
                                                    
                                                         switch: feeder, fused  | 
                                                
| 
                                                         sw_fused_isolated  | 
                                                    
                                                         switch: feeder, fused, isolated  | 
                                                
| 
                                                         sw_general  | 
                                                    
                                                         switch: feeder, general  | 
                                                
| 
                                                         sw_knife  | 
                                                    
                                                         switch: knife type  | 
                                                
PLS_DISPLAY
This library includes two genies that provide data row items for equipment.
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         equiplistitem  | 
                                                    
                                                         data row for the equipment tag list  | 
                                                
| 
                                                         EquipValueItem  | 
                                                    
                                                         data row for the equipment popup  | 
                                                
PLS_GEN_BASE_1 / PLS_GEN_BASE_2
These libraries include a variety of "parts" related to generators, motors, and transformers.
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         chassis_ground  | 
                                                    
                                                         chassis ground  | 
                                                
| 
                                                         Dev_Base  | 
                                                    
                                                         device base  | 
                                                
| 
                                                         es_inc  | 
                                                    
                                                         earth switch, incomer  | 
                                                
| 
                                                         es_out  | 
                                                    
                                                         earth switch, feeder  | 
                                                
| 
                                                         Gen_1  | 
                                                    
                                                         generator, option 1  | 
                                                
| 
                                                         Gen_2  | 
                                                    
                                                         generator, option 2  | 
                                                
| 
                                                         gen_AC  | 
                                                    
                                                         generator: AC  | 
                                                
| 
                                                         gen_DC  | 
                                                    
                                                         generator: DC  | 
                                                
| 
                                                         genset  | 
                                                    
                                                         engine-generator  | 
                                                
| 
                                                         ground  | 
                                                    
                                                         ground  | 
                                                
| 
                                                         Motor_1  | 
                                                    
                                                         motor, option 1  | 
                                                
| 
                                                         Motor_2  | 
                                                    
                                                         motor, option 2  | 
                                                
| 
                                                         motor_ac  | 
                                                    
                                                         motor: AC  | 
                                                
| 
                                                         motor_dc  | 
                                                    
                                                         motor: DC  | 
                                                
| 
                                                         motor_synch  | 
                                                    
                                                         motor: synchronous  | 
                                                
| 
                                                         SL_Base  | 
                                                    
                                                         circuit breaker base symbol  | 
                                                
| 
                                                         sl_br_in  | 
                                                    
                                                         circuit breaker line in, non-drawout  | 
                                                
| 
                                                         sl_br_out  | 
                                                    
                                                         circuit breaker line out, non-drawout  | 
                                                
| 
                                                         SL_Bustie  | 
                                                    
                                                         bus tie  | 
                                                
| 
                                                         SL_CommLoss  | 
                                                    
                                                         comms loss  | 
                                                
| 
                                                         SL_Discrepancy  | 
                                                    
                                                         position discrepancy  | 
                                                
| 
                                                         sl_harmonic_filter_1  | 
                                                    
                                                         harmonic filter 1  | 
                                                
| 
                                                         sl_harmonic_filter_2  | 
                                                    
                                                         harmonic filter 2  | 
                                                
| 
                                                         SL_In  | 
                                                    
                                                         incoming bus  | 
                                                
| 
                                                         SL_Local  | 
                                                    
                                                         local, rather than remote control  | 
                                                
| 
                                                         SL_Out  | 
                                                    
                                                         feeder  | 
                                                
| 
                                                         SL_Tripped  | 
                                                    
                                                         tripped  | 
                                                
| 
                                                         Test_CB_Control  | 
                                                    
                                                         health test for the circuit breaker control  | 
                                                
| 
                                                         transformer_1_in  | 
                                                    
                                                         transformer 1: general, on-line  | 
                                                
| 
                                                         transformer_1_in_y  | 
                                                    
                                                         transformer 1: star (wye), on-line  | 
                                                
| 
                                                         transformer_1_out  | 
                                                    
                                                         transformer 1: general, off-line  | 
                                                
| 
                                                         transformer_1_out_d  | 
                                                    
                                                         transformer 1: delta, off-line  | 
                                                
| 
                                                         transformer_1_out_y  | 
                                                    
                                                         transformer 1: star (wye), off-line  | 
                                                
| 
                                                         transformer_2_in  | 
                                                    
                                                         transformer 2: general, on-line  | 
                                                
| 
                                                         transformer_2_in_Y  | 
                                                    
                                                         transformer 2: star (wye), on-line  | 
                                                
| 
                                                         transformer_2_out  | 
                                                    
                                                         transformer 2: general, off-line  | 
                                                
| 
                                                         transformer_2_out_D  | 
                                                    
                                                         transformer 2: delta, off-line  | 
                                                
| 
                                                         transformer_2_out_Y  | 
                                                    
                                                         transformer 2: star (wye), off-line (no 2 IN D? or 1 IN D?)  | 
                                                
PLS_GEN_CMD_1 / PLS_GEN_CMD_2
These libraries include genies that control display of popups and values:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         CmdDetail  | 
                                                    
                                                         provides access to the equipment detail popup  | 
                                                
| 
                                                         cmddetail_meter  | 
                                                    
                                                         provides access to the meter detail popup  | 
                                                
| 
                                                         Control  | 
                                                    
                                                         control in a circuit breaker  | 
                                                
| 
                                                         value  | 
                                                    
                                                         value section of a circuit breaker  | 
                                                
| 
                                                         value_meter  | 
                                                    
                                                         value section of a meter  | 
                                                
PLS_GEN_EQ_1 / PLS_GEN_EQ_2
These libraries include the general equipment used to make up generators, motors, and transformers:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         busbar_horz  | 
                                                    
                                                         horizontal busbar  | 
                                                
| 
                                                         busbar_vert  | 
                                                    
                                                         vertical busbar  | 
                                                
| 
                                                         gen_ac  | 
                                                    
                                                         generator: AC  | 
                                                
| 
                                                         gen_dc  | 
                                                    
                                                         generator: DC  | 
                                                
| 
                                                         gen_nd_1  | 
                                                    
                                                         generator 1: no current designation  | 
                                                
| 
                                                         gen_nd_2  | 
                                                    
                                                         generator 2: no current designation  | 
                                                
| 
                                                         mot_ac  | 
                                                    
                                                         motor: AC  | 
                                                
| 
                                                         mot_dc  | 
                                                    
                                                         motor: DC  | 
                                                
| 
                                                         mot_nd_1  | 
                                                    
                                                         motor 1: no current designation  | 
                                                
| 
                                                         mot_nd_2  | 
                                                    
                                                         motor 2: no current designation  | 
                                                
| 
                                                         mot_syn  | 
                                                    
                                                         motor, synchronous  | 
                                                
| 
                                                         trans_nd_1  | 
                                                    
                                                         transformer 1: no connection designation  | 
                                                
| 
                                                         trans_nd_2  | 
                                                    
                                                         transformer 2: no connection designation  | 
                                                
| 
                                                         trans_sd_1  | 
                                                    
                                                         transformer 1: star-delta (wye-delta)  | 
                                                
| 
                                                         trans_sd_2  | 
                                                    
                                                         transformer 2: star delta (wye-delta)  | 
                                                
| 
                                                         trans_ss_1  | 
                                                    
                                                         transformer 1: star-star (wye-wye)  | 
                                                
| 
                                                         trans_ss_2  | 
                                                    
                                                         transformer 2: star-star (wye-wye)  | 
                                                
PLS_IEC_BASE_1 / PLS_IEC_BASE_2
These libraries include a variety of symbols for IEC equipment:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         sl_cap_bank_tuned_3  | 
                                                    
                                                         capacitor bank 3: tuned  | 
                                                
| 
                                                         sl_cap_bank_tuned_4  | 
                                                    
                                                         capacitor bank 4: tuned  | 
                                                
| 
                                                         sl_capacitor  | 
                                                    
                                                         capacitor  | 
                                                
| 
                                                         sl_capacitor_vari  | 
                                                    
                                                         capacitor, variable  | 
                                                
| 
                                                         sl_closed  | 
                                                    
                                                         closed switch  | 
                                                
| 
                                                         sl_contact_nc  | 
                                                    
                                                         contact break  | 
                                                
| 
                                                         sl_ct  | 
                                                    
                                                         contact  | 
                                                
| 
                                                         sl_fuse_1  | 
                                                    
                                                         fuse, option 1  | 
                                                
| 
                                                         sl_fuse_2  | 
                                                    
                                                         fuse, option 2  | 
                                                
| 
                                                         SL_Head  | 
                                                    
                                                         head  | 
                                                
| 
                                                         sl_head_2  | 
                                                    
                                                         head  | 
                                                
| 
                                                         sl_in_cb_rack  | 
                                                    
                                                         incoming, circuit breaker when racked out, plug  | 
                                                
| 
                                                         SL_In_Rack  | 
                                                    
                                                         incoming, circuit breaker when racked out, socket  | 
                                                
| 
                                                         sl_in_sw_hd_isol  | 
                                                    
                                                         incoming, switch head, isolated  | 
                                                
| 
                                                         sl_in_sw_head  | 
                                                    
                                                         incoming, switch head  | 
                                                
| 
                                                         sl_inductor  | 
                                                    
                                                         inductor  | 
                                                
| 
                                                         sl_inductor_adjust  | 
                                                    
                                                         inductor, adjustable  | 
                                                
| 
                                                         SL_Open  | 
                                                    
                                                         open  | 
                                                
| 
                                                         sl_out_cb_rack  | 
                                                    
                                                         feeder, circuit breaker when racked out, plug  | 
                                                
| 
                                                         SL_Out_Rack  | 
                                                    
                                                         feeder, circuit breaker when racked out, socket  | 
                                                
| 
                                                         sl_resistor  | 
                                                    
                                                         resistor  | 
                                                
| 
                                                         sl_resistor_adjust  | 
                                                    
                                                         resistor with adjustable contact  | 
                                                
| 
                                                         sl_resistor_vari  | 
                                                    
                                                         resistor, variable  | 
                                                
| 
                                                         sl_sw_static_1  | 
                                                    
                                                         static switch 1  | 
                                                
| 
                                                         sl_sw_static_2  | 
                                                    
                                                         static switch 2  | 
                                                
PLS_IEC_CB_1 / PLS_IEC_CB_2
These libraries include high-voltage drawout circuit breakers:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         hv_cb_bus_dr_c  | 
                                                    
                                                         high-voltage drawout circuit breaker, remote control  | 
                                                
| 
                                                         hv_cb_bus_dr_nc  | 
                                                    
                                                         high-voltage drawout circuit breaker, no remote control  | 
                                                
| 
                                                         hv_cb_bus_nd_c  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, remote control  | 
                                                
| 
                                                         hv_cb_bus_nd_nc  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, no remote control  | 
                                                
| 
                                                         hv_cb_fd_dr_c  | 
                                                    
                                                         high-voltage, drawout circuit breaker, remote control, earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_dr_nc  | 
                                                    
                                                         high-voltage, drawout circuit breaker, no remote control, earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_nd_c  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, remote control, earth at bottom  | 
                                                
| 
                                                         hv_cb_fd_nd_nc  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, no remote control, earth at bottom  | 
                                                
| 
                                                         hv_cb_inc_dr_c  | 
                                                    
                                                         high-voltage, drawout circuit breaker, remote control, earth at top  | 
                                                
| 
                                                         hv_cb_inc_dr_nc  | 
                                                    
                                                         high-voltage, drawout circuit breaker, no remote control, earth at top  | 
                                                
| 
                                                         hv_cb_inc_nd_c  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, remote control, earth at top  | 
                                                
| 
                                                         hv_cb_inc_nd_nc  | 
                                                    
                                                         high-voltage, non-drawout circuit breaker, no remote control, earth at top  | 
                                                
| 
                                                         hv_cb_nes_dr_c  | 
                                                    
                                                         high-voltage drawout circuit breaker, remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_dr_nc  | 
                                                    
                                                         high-voltage drawout circuit breaker, no remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_nd_c  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, remote control, no earth  | 
                                                
| 
                                                         hv_cb_nes_nd_nc  | 
                                                    
                                                         high-voltage non-drawout circuit breaker, no remote control, no earth  | 
                                                
PLS_IEC_SW_1 / PLS_IEC_SW_2
These libraries include IEC-style switches:
1 = small size
2 = large size
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         sw_general  | 
                                                    
                                                         general switch  | 
                                                
| 
                                                         sw_isolated  | 
                                                    
                                                         isolated switch  | 
                                                
PLS_METER
This library includes meter symbols.
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         circuit monitor  | 
                                                    
                                                         Power Operation circuit monitor  | 
                                                
| 
                                                         egx  | 
                                                    
                                                         Power Operation EGX  | 
                                                
| 
                                                         generic_meter  | 
                                                    
                                                         generic meter  | 
                                                
| 
                                                         ion_7650  | 
                                                    
                                                         ION 7650 meter  | 
                                                
| 
                                                         micrologic  | 
                                                    |
| 
                                                         power_meter  | 
                                                    
                                                         Power Operation power meter  | 
                                                
| 
                                                         quantum  | 
                                                    |
| 
                                                         sepam  | 
                                                    
ITEM1
This library includes miscellaneous symbols.
| 
                                                         Genie Abbreviation  | 
                                                    
                                                         Description  | 
                                                
|---|---|
| 
                                                         Item1  | 
                                                    
                                                         value type and units block for a circuit breaker  | 
                                                
| 
                                                         Item2  | 
                                                    
                                                         value type and units block for a circuit breaker  | 
                                                
| 
                                                         tab1  | 
                                                    
                                                         menu tab  | 
                                                
| 
                                                         Tab2  | 
                                                    
                                                         menu tab  |