Settings and Diagnostics UI
Settings and Diagnostics consists of the Notifications Settings configuration, migration, diagnostics, and licensing features and information.
                                            
                                        
| 1 | Settings navigator pane. Select a setting category to work with that setting. For more information, see Configuring Notifications. | 
| 2 | System diagnostics and settings. For more information, see Troubleshooting Notifications. | 
| 3 | 
                                                         The server's license status.  |