Alarms references
This section contains reference information related to using Alarms.
Use the links in the following table to find the content you are looking for:
| Topic | Content | 
|---|---|
| Alarms UI | Contains detailed information on the Alarms UI. | 
| Waveforms UI | Contains detailed information on the Waveforms UI. | 
| Timeline Analysis UI | Contains detailed information on the Timeline Analysis UI. | 
| Alarm to Incident Mapping | Details the mapping of alarm types to Incidents. | 
| Alarms terminology | A list of commonly used terms related to Alarms in Power Operation. |