Busbar

A busbar is a metallic strip or bar (typically copper, brass or aluminium) that conducts electricity within a switchboard, distribution board, substation, battery bank, or other electrical apparatus to make a common connection between several circuits in a system.

Busbar has only one bind property; BusColor.

The graphic representation of the default position and the bind property is shown in the below table:

Bind Property Description Graphic
NA Busbar is in default position.
BusColor Sets the bus color.