Transformer

A transformer is a device that transfers electrical energy from one electrical circuit to another without any change of frequency through the process of electromagnetic induction.

The different types of transformers that are supported in the Power Operation are:

  • Trans_nd_1
  • Trans_nd_2
  • Trans_sd_1
  • Trans_sd_2
  • Trans_ss_1
  • Trans_ss_2

The bind properties available for transformer are:

  • TopBusColor
  • BottomBusColor

The graphic representation of the default position and the bind properties is shown in the below table:

Bind Property Description Graphic
NA Transformer is in default position.
TopBusColor Sets the bus color.
BottomBusColor
  • TopBusColor
  • IsTripped
  • IsClosed
  • RkdPos
  • BottomBusColor
  • EarthSwitchClosed