Utilities
Utility is a commercial entity that owns and operates equipment and facilities for the generation, transmission, and distribution of electric energy.
The different types of utilities that are supported in the Power Operation are:
- Util_nd_1
- Util_nd_2
Utility has only one bind property; BusColor.
The graphic representation of the default position and the bind property is shown in the below table:
Bind Property | Description | Graphic |
---|---|---|
NA | Utility is in default position. |
![]() |
BusColor | Sets the bus color. |
![]() |