Application Services Logging
Logging Level:
This feature turns on extra diagnostic information that can be useful when diagnosing problems that occur in application services or its hosted applications (such as LiveView). Choose the level of logging to be used in all applications. Debug and Verbose increase the amount of information that is logged during runtime for applications such as Basic Reports and LiveView.
- Normal: Use when the project is live.
- Debug: includes additional logging statements (in the Windows event log named PowerLogic). This logging should not affect performance in the system during runtime.
- Verbose: releases additional diagnostic information, such as large lists, that could affect system performance.
Service Inventory:
This is a read-only list of Web services hosted by the Schneider Electric CoreServiceHost, details about them, and whether they are running.