LiveView Energy Readings
This table displays accumulated energy readings for a single device. Data is accumulated beginning with the last energy reset for the device.
Energy values, will be according to one of these accumulation methods:
Absolute (unsigned): The device stores positive energy values, regardless of the direction of power flow. The energy value increases, even during reverse power flow.
Signed: The device stores both positive and negative energy values. The energy value increases or decreases, depending on the direction of the power flow.
After opening the live view energy readings table, choose the device you want and set the update interval for this table. Select Display Table.
The live view energy readings table provides these accumulated readings:
- real energy (kWHr)
 - reactive energy (kVARHr)
 - apparent energy (kVAHr)