LiveView Energy Summary
This summary displays an energy summary for your system devices. Use the information from this table to help monitor the system's energy consumption.
After opening the energy summary template, you set the update interval for this summary. You can also add or remove devices from the summary.
Make your selections, and select Display Table.
The energy summary provides this data:
- real power (kW)
 - reactive power (kVAR)
 - apparent power (kVA)
 - block demand real power (kW)
 - thermal demand real power (kW)
 - peak block demand real power (kW)
 - peak thermal demand real power (kW)
 - block demand real power predicted (kW)
 - thermal demand real power predicted (kW)